12/28/2020 2:38 PM | |
Joined: 3/11/2019 Last visit: 4/26/2024 Posts: 1378 Rating: (244) |
Dear Peter, thermocouples always needs a reference junction. If parameter is set to "fixed", the reference temperature is set to 0°C means you will need exactly this temperature at the connecting point. The easiest way is to use "internal reference junction" but therefore a baseunit with internal temperature sensor is needed. In general, the following FAQ is helpful: What do you have to watch out for when using thermocouples if the expected value is not displayed?
Maybe this helps regards sancruz |
Feedback appreciated, please rate |
|
Follow us on