9/26/2014 9:14 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, 6RA80 manual for F60062 says as below
Message value: %1 Drive object: DC_CTRL Reaction: OFF2 (NONE, OFF1, OFF3) Acknowledge: IMMEDIATELY Cause: Communication to one of the two voltage sensing devices is faulted or interrupted.Fault value (r0949, decimal interpretation): 1: Armature voltage sensing 2: Field voltage sensing Note: r50047[1]: Counter CRC error, armature r50047[2]: Counter, communication error, armature r50047[3]: Counter, CRC error, field r50047[4]: Counter, communication error, field Remedy: POWER ON all components (switch the power off and then back on again). |