6/6/2014 8:37 AM | |
Posts: 28 Rating: (0) |
hi sir, in the old driver p081=0, in my list i attachment, that's the parameters have changed for the default parameters.i see some parameter is set automatically during the field-weakening optimization run (P051=27) sush as: p117 p118 p119 so when i upgrad to 6RA80 i need to choose a p50051=27 or not? because motor have no encoder or tacho |
6/6/2014 9:02 AM | |
Posts: 28 Rating: (0) |
my applycation need to control level speed motor from man setpoint(-10v to 10v),no need to feeback so i optimizations p=24,p=25 ,p=26 .its is enough ? |