6/29/2018 3:50 PM | |
Joined: 8/25/2011 Last visit: 4/16/2024 Posts: 29 Rating: (4) |
Hi, I take it that the master will be in purely speed control with no torque limit? You can set the slave to torque control by setting p587=1 if you take connector K0153 ( output from speed controller) to an analogue output on the master then input this into an analogue input on the slave drive. Use this analogue input into P486 (torque setpoint on the slave) I assume both bridle drives are the same size. Make sure the the reference torque parameter P354 is the same to match the scaling for the torque signal. I have attached some pages from the manual to show the signal flow. AttachmentMaster Slave.pdf (225 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on