5/31/2016 1:58 PM | |
Posts: 5 Rating:
|
Jacku, Tak, jest podpięta diodka której nie możemy zgasić nawet używając funkcji "Force". Z tego powodu użyliśmy woltomierza i okazało się, że na wejściu zostaje 6V, niezależnie od obciążenia. Na module typu standard wszystko działało poprawnie. Pozdrawiam ========================================= Yes, there is a output diode which we cannot turn off even if output is forced to 0. In this case we checked by multimeter what is happening there, and it appears there always is 6V. On standard module everything works properly. Regards |
5/31/2016 2:42 PM | |
Joined: 9/23/2005 Last visit: 2/27/2021 Posts: 3171 Rating:
|
Can you try to connect resistance ca. 50 ohm in parallel? Or Zener diode in series? The issue is due to test functions this module has. They can't be switched off. The output is forceing ca. 0.5 mA to the load at "0". If load is >=12k ohm output goes up to 6 V. |
Regards, |
|
This contribution was helpful to
2 thankful Users |
6/2/2016 2:42 PM | |
Posts: 5 Rating:
|
Thank you for solution. We used relay on this output and everything work properly now. |
This contribution was helpful to
2 thankful Users |
Follow us on