7/1/2014 4:30 PM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating: (37) |
Hi! PTO means power-take-off? Or? Please describe your question more detailed. |
7/1/2014 5:52 PM | |
Joined: 9/27/2006 Last visit: 9/20/2024 Posts: 12282 Rating: (2684)
|
Hello musketeer; I would presume you are asking about Pulse Train Outputs, in order to control stepper or servo motors. If this is the case you should tell us a bit more of what you need, in terms of pulse outputfrequency and voltage level. There are various ways of doing this, depending on those parameters. For very high speed pulse trains you would have to look into theFM 352-5, which would give you the outputs you need but which requires a good deal of parametrization and programming skills: FM 352-5 high-speed Boolean processor Have a look at the technical specifications of the FM and tell us if it provides what you would need. If not come back with more details on your application. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
7/5/2014 12:44 PM | |
Joined: 4/2/2014 Last visit: 1/25/2024 Posts: 52 Rating: (1) |
thanks for reply. i want to drive 7 servo motor using 7 different pulse train output that is the need of application. |
7/6/2014 10:56 AM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Hello Musketeer You can use the Following : You will have to install these modules in a ET200S Profibus Slave Rack.
|
Last edited by: Navnag at: 7/6/2014 10:57 AMThere is no such thing as the last bug in a program |
|
Follow us on