Industry Online Support
Technical Forum
6/11/2012 4:56 PM | |
Joined: 12/14/2010 Last visit: 6/28/2023 Posts: 160 Rating: (6) |
Hi GoForIT, The thing is that the WinCC Images Hierarchy (from Tree Manager Editor) and the Technological Hierarchy (from Component List Editor) differ. If you are working with a PCS 7 project, read here (maybe first you need to translate this page to english): https://support.automation.siemens.com/WW/llisapi.dll?func=ll&objId=22014044&nodeid0=10805583&load=treecontent&switchLang;22015775;5.x=34&switchLang;22015775;5.y=4&lang=en&siteid=cseus&aktprim=0&objaction=csview&extranet=standard&viewreg=WW&display=p if you are working with a WinCC project and you create the WinCC Images Hierarchy (of course, manually) from the Tree Manager, then: "open the Componet List Editor -> Left Click on Edit menu ->Left Click on Create meausing point. -> and fill at list the following two fields: -Measuring Point = "The name of the structure corresponding to the faceplate"; - Entry point picture = "The name of the image you need permission for the faceplate "; tell me if this served you. best regards |
Follow us on