8/28/2012 8:09 AM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
Have a look on this link Communication s7-200 with Field PG M |
Ammy |
|
8/29/2012 7:26 AM | |
Posts: 9 Rating: (0) |
thanks for the feed back,now my problem is plc s7-200 port is connected with tp177 hmi device,where or which port i will connect my PG. pl help me. |
11/11/2012 6:37 AM | |
Posts: 10 Rating: (0) |
Hello, Is there any solution for this thread ? I'm facing the same problem. Thanks.
|
11/12/2012 9:07 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (713)
|
Hello, Use this connector at CPU to connect your panel: PB CONNECTOR, 90 DEGREE, WITH PG SOCKET Regards, Marcjan |
Problem solved? |
|
10/31/2016 3:56 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by borg112 is split to a separate thread with the subject Profibus DP connector (6ES7972-0BB70-0XA0) works on CPU 226?. Best regards |
Follow us on