9/17/2012 7:10 AM | |
Joined: 10/3/2010 Last visit: 10/17/2024 Posts: 1562 Rating: (192) |
Did you check the compatibility list (including the remarks beneath the listed table)? http://support.automation.siemens.com/WW/llisapi.dll/csfetch/21927773/WinCC_V70_compatibility_list_e.pdf?func=cslib.csFetch&nodeid=48697165 or http://support.automation.siemens.com/WW/view/en/21927773 WinCC 7 SP1 is only supported on Server 2003 SP2 or Server 2003 R2 SP2 (both Standard and Enterprise Edition). WinCC 7 SP2 is the only one also supporting Server 2008 SP2 but with following remarks: -both Standard and Enterprise Edition -Please consider the following link for a optionally downgrade of Windows Server 2008 R2: http://www.microsoft.com/windowsserver2008/en/us/downgrade-rights.aspx -Microsoft Windows Server 2008 without Hyper-V is not allowed I think you need a WinCC installation CD with SP2 already included. Brgds. |
Last edited by: SteBo at: 9/17/2012 7:13 AMB r g d s , |
|
12/30/2015 10:23 AM | |
Joined: 9/1/2005 Last visit: 10/14/2024 Posts: 4109 Rating: (195) |
New question published by a15 is split to a separate thread with the subject wincc7 sp2 supported for window 8?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on