Industry Online Support
Technical Forum
6/20/2011 10:22 AM | |
Joined: 9/18/2006 Last visit: 2/6/2024 Posts: 589 Rating: (64) |
Hi. From the PLC (V28001010.0 = 1) output (DO9) is set? If the output (DO9) from the PLC is setting, you can choose to set the signals: V28001009.0 or V28001011.0 or V29001004.0 I can not verify. Best regards. AttachmentSignals to fast inputs and outputs.pdf (91 Downloads) |
Last edited by: pfuser at: 6/20/2011 10:31 AM |
|
Follow us on