Industry Online Support
Technical Forum
8/25/2012 6:37 AM | |
Joined: 10/27/2009 Last visit: 3/15/2024 Posts: 455 Rating: (77) |
HI; There's a tool available: "CreateMyConfig 4.5" (former names: "UpdateAgent" and "SINUCOM Installer"). Each of these three program packages contains the programs DIFF, EXPERT and TOPO. (The older versions contains these three subprograms with different names) By using the DIFF You can open and compare many archives at the same time. You can: - compare machine parameters ond data (MachineData, ENC-compdata, tooldata, R-parameters....) - compare the programs inside the archive (USER-cyles, OEM-cycles, MPF's...) - compare drive data - export the result of the comparison e.g.in EXCEL. The CMC 4.5 was developed basically for handling and configuration SIN840Dsl but the DIFFprogram cover the comparison of SIN840D-archives as well. Please contact Your nearest SIEMENS-office to get an official version of "CreateMyConfig". hope that helps CNC600
AttachmentCreate MyConfig - Manual.pdf page14.pdf (143 Downloads) |
Last edited by: CNC600 at: 8/25/2012 7:05 AMTo get an overview I attached one page from Manual: NC-Data in comparison in the background, SINAMICS-Data comparison in the front Last edited by: CNC600 at: 8/25/2012 6:40 AMhope that helps |
|
This contribution was helpful to2 thankful Users |
Follow us on