6/14/2017 1:00 PM | |
Posts: 46 Rating: (0) |
Hi I have a machine(Chiron FZ15W) which have safety. It has come to my factory witthout 4º and 5º axis. It is supposed that it is ready to conect the motors and work(a technician has come to configure it) The motors that I want to connect are different. The machine is parametriced for 1FK7063-xAF7x-xCxx and the motors that I have are 1FK7042-2AF71-1CG2. If I connect the motors, the machine gives me some error (encoder errors I think) I think that I need to change the topology to tell to the machine which type of motors are conected but I don´t know how tom make it. I don´t know if the safety could give me problems, I think that I will have to parametrize the 4º and 5º axis again. I upload some pictures of the problem I have TCU20.2 Could someone help me? Thanks Attachmentalarm.zip (50 Downloads) |
Follow us on