2/26/2016 11:52 AM | |
Posts: 62 Rating: (0) |
Hello. I have the same problem SPEC_CNC. My configuration is DC motor with ADI4, Sinamics DCM and Sinumerik 840dsl A DC motor mx speed is 2400rpm We have one encoder on spindl, encoder resolution is 2500 We have 4 gears 1. gear is S15 - S430 the ratio is 1/5,5777 2. gear is S23 - S666 the ratio is 1/3,604 3. gear is S40 - S1170 the ratio is 1/2,052 4.gear is S63 - S1810 the ratio is 1/1,326 Problem is that now is spindle max speed 1600rpm. And when I put in mda S1800 the max speed is 1600rpm when i have spindle override on 60%. On 50% override i have abaot 1300rpm. If i put my override on 100% is the same like 60% My MDA configuration is like that: MD31050[0] = 10 MD31050[1] = 10 MD31050[2] = 10 MD31050[3] = 10 MD31050[4] = 10 MD31060[0] = 56 MD31060[1] = 56 MD31060[2] = 36 MD31060[3] = 20 MD31060[4] = 13 MD32250 = 120% MD32260 = 2400rpm Can somebody help me. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/26/2016 1:05:25 PMNew subject after splitting |
|
2/26/2016 2:45 PM | |
Posts: 62 Rating: (0) |
hello thank you for your reply. if i setup parameter MD32260 =2400 is my maximal speed 1200rpm. Parameter md32250 must bi 100%? |
2/26/2016 3:21 PM | |
Posts: 62 Rating: (0) |
There is my nc archive. AttachmentNC26022016.zip (179 Downloads) |
2/29/2016 8:44 AM | |
Posts: 62 Rating: (0) |
Hello, sorry i atach a wrong NC archive, This is correct NC arhive. The maximal speed of spindle is 922rpm. AttachmentNC29022016.zip (180 Downloads) |
Follow us on