2/8/2013 8:15 PM | |
Joined: 7/2/2010 Last visit: 1/22/2024 Posts: 50 Rating: (0) |
I managed to run the drive without OP anyway i will need this program to download it to the new OP7. Attached is the only information i could get from commissioning manual.
AttachmentCommissioning instructions-E.pdf (508 Downloads) |
9/1/2014 5:27 PM | |
Joined: 7/12/2012 Last visit: 11/21/2023 Posts: 25 Rating: (0) |
Hello Emiljani, Is the problem solved? I have backup OP7 program with the same order number. Regards, MYH |
Follow us on