2/13/2013 10:31 AM | |
Joined: 10/22/2008 Last visit: 4/25/2024 Posts: 365 Rating: (5) |
Hello LOGO! users, In attachement I gave *.lld file with my problem. On first look it seems to be an empty program in ladder format. But if you would like to download it to the device the compiler gives an information there are block not connected. In simulator it is also possible to simulate Q12 that is not used in proram. My qiestion is how to remove the bloscks? I don't want to change to fbd view becauseof the mess it gives. best regards Attachmentabcd.zip (138 Downloads) |
2/13/2013 10:51 AM | |
Posts: 2930 Rating: (432)
|
Hi, if you have the lates verison, then the only way I know is to change to FBD and remove the blocks. You than can change back to Ladder. Regards |
2/13/2013 11:36 AM | |
Joined: 10/22/2008 Last visit: 4/25/2024 Posts: 365 Rating: (5) |
but if I do that the program will become really messy. |
5/20/2016 9:55 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by Johnluck is split to a separate thread with the subject How do I use simulator in master to master network program?. Best regards |
Follow us on