2/27/2013 9:38 PM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
All computers are found in the network? You have to find them by computer name, not only by IP address.. All users are the same, with same password? As of v6.0, Its recommended to use a client with own project, rather than use a so called "uniclient" (client without own project). Don't know if problems could arise from it Did you set up the correct authorization rights for your users? -> 1001 Activate remote Package loaded succesfully? |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
6/18/2015 2:49 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
|
Follow us on