3/5/2013 8:44 AM | |
Joined: 2/10/2010 Last visit: 11/24/2023 Posts: 77 Rating: (0) |
Dear experts, Is it possible to use WinCC server redundancy with Windows Server 2008 32-bit?
|
3/5/2013 12:09 PM | |
Posts: 1530 Rating: (59)
|
Hello rajudon, as you don't mention which version of WinCC Redundancy you are working with I would suggest you look into: With what are SIMATIC WinCC V7.x, V 6.x and V5.x compatible? Either you take Compatibility-Tool at the beginning of this FAQ, or you look into Excel-List at end of it. Best regards Bizur |
3/5/2013 3:35 PM | |
Joined: 2/10/2010 Last visit: 11/24/2023 Posts: 77 Rating: (0) |
Sorry, I missed the version . the Version is 7.0 SP2. I have checked the compatibilty. But, neither the compatibility tool or the excel list says the compatibility of WinCC V7.0 SP2 Redundant Systems with the windows version. Those only say the compatibility of the WinCC V7.0 SP2 with the windows server 2008 32-bit. Does it imply all the features (redundancy also)are compatible? In one the document on WinCC V7.0 SP2 Redundant Systems, it is mentioned that "The redundant servers must be equipped with Windows 2003 Server. The client PCs must be equipped with Windows XP or Windows Vista." Check the attached document, Page 8 of 50. We are facing a problem with WinCC V7.0 SP2 Redundancy with Windows Server 2008. When the master server goes down, the tag values on the client gets updated from the second server. But, we are not being able to change the screen on the client. The screen which was open earlier (when master server was healthy), gets the tag values updated continously from the redundant server.But, no further screen change is possible. We have Windows 7 on the client. Does it have any solution? regards, rajudon AttachmentRedundancy.pdf (88 Downloads) |
3/7/2013 9:34 AM | |
Joined: 2/10/2010 Last visit: 11/24/2023 Posts: 77 Rating: (0) |
Dear Bizur, the attached file contains the OS and WinCC versions. The architecture is redundant server-client. with regards, rajudon AttachmentInstalled Software.pdf (94 Downloads) |
Follow us on