Industry Online Support
Technical Forum
6/24/2013 12:53 PM | |
Posts: 93 Rating: (13) |
Please explain elaboratoly. Problem is pretty much unclear. Also if you can expain through some diagram. Thanks & regards. |
6/24/2013 1:02 PM | |
Joined: 10/3/2010 Last visit: 4/29/2024 Posts: 1552 Rating: (188) |
Question seems already answered by Saravana kumar Only extra can be to remove clients in the list on the PC that you want to simulate or work on the project but it's not a must. Brgds. |
B r g d s , |
|
6/25/2013 4:55 AM | |
Posts: 20 Rating: (0) |
Hi Saravana, Thank you for the help, yes, I have to change it with my computer name. Thanks in advance. Best regards, Arsy
|
Follow us on