7/13/2013 2:25 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (272) |
Hello, As you said you want to protect some screens than it is also possible to do it without using User Administration. Here you will find all the detailed information with Example. How can you create a protected user screen without using user administration? With use of user Administration , it is only possible via downloading again on invalid attempts. A user enters an incorrect password three times in succession, that user is entered in the "Unauthorized" group in the user administration. Only a user with administrator rights can reassign that user to a user group. Why can you no longer log on to the operator panel (or WinCC flexible Runtime)? Hope this helps. |
VANDE MATARAM..... |
|
This contribution was helpful to1 thankful Users |
Follow us on