7/22/2013 7:41 AM | |
Joined: 2/20/2012 Last visit: 5/11/2023 Posts: 62 Rating:
|
Dear Experts, I am not sure what is happening with client OS here in PCS7 V8.0 SP1 system. Attached are the screenshots of Server and client pictures. Server is showing the screens and working well. But the client is not showing the area buttons properly. But it is communicating to the servers and can see the Redundant server display state at the top right (Green in colour). Below are the steps that I tried to solve it but with no luck. I ran the OS project editor once again and started. Not working Deleted the project in OS client. Re-downloaded the project - no luck. Generated Server data once again - assigned itt o the Client in ES and re-downloaded the Server and Client projects - still no luck. Please let me know if anyone had this problem, Need to solve ASAP. Thanks and regards, Sudheendra Attachmentpictures.zip (504 Downloads) |
7/22/2013 1:37 PM | |
Joined: 2/20/2012 Last visit: 5/11/2023 Posts: 62 Rating:
|
Hi.. |
7/22/2013 11:07 PM | |
Posts: 2661 Rating:
|
Did you set the Standard server (SSM & Alarms)on the client? |
7/23/2013 7:32 AM | |
Joined: 2/20/2012 Last visit: 5/11/2023 Posts: 62 Rating:
|
Yes. I have assigned the SSM and Alarms. I deleted all the clients and reconfigured it. Still no solutions. |
7/23/2013 12:04 PM | |
Joined: 7/13/2009 Last visit: 6/3/2024 Posts: 137 Rating:
|
Hi Sudheendra, Configure ES as OS client and check.
|
Thanks and Regards |
|
7/24/2013 12:43 AM | |
Posts: 2661 Rating:
|
Is the Windows username/password same for both Client and Server? |
Follow us on