9/4/2008 3:09 PM | |
Posts: 487 Rating: (45) |
You are allowed to create custome table on the SQL server database that comes with WinCC as long as the table is used in conjuction with the WinCC project. I have done this before in consultation with Siemens. Please check the FAQ below. http://support.automation.siemens.com/WW/view/en/23680533 |
9/5/2008 9:55 AM | |
Posts: 487 Rating: (36) |
Hi Could install MySql . Eric |
9/8/2008 9:16 PM | |
Posts: 168 Rating: (49) |
Furthermore, if you're right, I think Siemens should change the name of WinCC Optional Pack "User Archive" to "Useless Archive" hum heh hum hum heh |
9/8/2008 11:05 PM | |
Posts: 487 Rating: (45) |
Dimicamp, I think you are confused between database and datatable. If you add your own datatable in RT DB, it is not creating your own table. I completely agree with the FAQ. The case discussedDOES NOT have 'own database' or 'third party applications'. Also please check the link below from A&D Mall. If you do not consider official training material from Siemens as "Official" about CAL license. https://mall.automation.siemens.com/DE/guest/index.asp?aktPrim=0&nodeID=10016159&mlfb=6AV6371%2D1ES06%2D0AX0&aktTab=4&lang=en I have also havesample programs from Siemens WinCC support with custom table in RT Database.
---- |
Last edited by: JMJ at: 9/8/2008 11:23 PM |
|
4/12/2011 4:03 PM | |
Posts: 11 Rating: (1) |
Hi, I'm not very clear about the conclusion. Can I "read" from the database but i can't "write/create" ? Regards |
Follow us on