Industry Online Support
Technical Forum
7/6/2012 9:24 AM | |
Posts: 15 Rating: (0) |
can we make a connection to S7200 plc ppi port with a MPI cable? thanks... |
7/6/2012 10:46 AM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147) |
Hello scanner.tr, Please explain which cable you want to use? Best regards, Wizard |
7/6/2012 10:48 AM | |
Posts: 8946 Rating: (999) |
An answer: Yes. |
7/6/2012 2:17 PM | |
Posts: 15 Rating: (0) |
thanks for your answers... the cable which we want to use is "pc adapter usb (6ES7972-0CB20-0XA0)" |
7/6/2012 3:00 PM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147) |
Hello scanner.tr, Yes, I agree with IBN-Service. It is possible to use USB-PC adapter. See also: New PC Adapter USB Now Available And see: Which configuration do you need for "PC Adapter USB" in conjunction with MicroWin and S7-200? Best regards, Wizard |
This contribution was helpful to1 thankful Users |
Follow us on