5/22/2012 9:10 AM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
Hi, From photograph it appears that all LED's of CPU is continusously ON, in that case you need to reaplce it.
|
5/22/2012 10:39 AM | |
Posts: 21 Rating: (0) |
Hi Wizard, Thanks for your info, I will go back and export the file again.
|
5/23/2012 12:30 PM | |
Posts: 21 Rating: (0) |
Dear all, First of all, I would like to thanks all of you for the information and suggestion provided. As concluded the information above, I think the best way is to change a new CPU card and during CPU replacement, I will check all the grounding point and also to ensure the firmware of CPU is the latest version. Meanwhile, can I have a better understanding of the diagnostic buffer I exported today? I have set the CPU to stop mode to export the file, I think Event 14 is the error log for this incident. (Kindly find attached diagnose file) and also below are the description of the Event 14. Event 14 of 100: Event ID 16# 4550 DEFECTIVE: internal system error No relevance for user (Z1): f102 Previous operating mode: RUN Requested operating mode: DEFECTIVE Internal error, Incoming event 07:41:42.536 AM 10/25/1995 Does it mean the CPU is defective? Thank you! AttachmentDiagnose_N2O#2_offline.zip (134 Downloads) |
Follow us on