5/6/2008 3:33 PM | |
Posts: 39 Rating: (0) |
hi everybody, I'm trying connect CPV 14-GE-ASI-8E8A-Z which have 8 input and 8 output to cp243-2 asi module but i can not find ASI-WIZARD for 8i/8Q atmicrowin. |
5/6/2008 4:02 PM | |
Joined: 9/27/2006 Last visit: 5/7/2024 Posts: 12257 Rating: (2666) |
Hello Obyone_2; I am surprised that there is such a thing as an As-i Wizard in MicroWin. I don't have access to MicroWin at the moment, so I would be grateful if you have any information to share about this. In my experience with As-i, through a DP/As-i Link or CP343-2 mastrer, it was considered un-macho to have recourse to anything but your brain (and pencil and paper) to map the As-i slaves. The following FAQ describes different aspects of the technique for the CP243-2: http://support.automation.siemens.com/WW/view/en/8826798 For your particular 8DI/8DO module, set its As-i slave address at 2, for example;then 8 bits of AI2 will be used for the 8DI signals, and 8 bits of AO2 will be connected to the 8 DO signals.You will access them through your program at the associated VBxxx you have selected for the As-i master module, offset by 2. Now if there is a Wizard to make this easier, I'm stunned! Hope this helps, Daniel Chartier |
5/6/2008 5:24 PM | |
Posts: 39 Rating: (0) |
where am i wrong? i am attaching the my connection for one slave. |
5/7/2008 7:25 AM | |
Joined: 9/27/2006 Last visit: 5/7/2024 Posts: 12257 Rating: (2666) |
Hello Obyone_2; I have looked at the following Festo manual: http://www.lcautomation.com/pdf/festo/festo_as-interface.pdf On page 12, it shows a table for: Permissible combinations in valve position allocation Could you look into any technical information about this valve coupler to find out if any special configuration should be prepared for the unit, and if you are allowed to modify it? Hope this helps, Daniel Chartier |
5/7/2008 12:49 PM | |
Posts: 39 Rating: (0) |
the picture i attached shows the terminal of festo valf group. |
Follow us on