Industry Online Support
Technical Forum
6/17/2009 9:36 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (306) |
Hello, The reference manaul of the system functions is here: http://support.automation.siemens.com/WW/view/en/1214574 SFC55 is restricted to records changing dynamic parameters Some SFC do not support new Profinet features. See p19 of this manual: "From Profibus DP to Profinet IO http://support.automation.siemens.com/WW/view/en/19289930 SFC 58/59 (write/read record in I/O) Replaced by: SFB53/52SFC55 (write dynamic parameters) Emulate using SFB53 I hope it is clear. Best is always to use the latest SFB/SFCs. They support Profibus and Profinet as well. |
Best regards |
|
This contribution was helpful to1 thankful Users |
Follow us on