Industry Online Support
Technical Forum
1/12/2010 7:21 AM | |
Joined: 5/12/2009 Last visit: 6/14/2022 Posts: 13 Rating: (0) |
Dear All, Currently i am working on a project in which we are using CPU 414-4H(6ES7-4HM14-0AB0) and CP 443-1 (6ES7443-1EX20-0XE0).I made the harware configuration and when i am compiling, it give error "inconsistent configuration". Few more query 1. I read on forum that for CP 443-1 (6ES7443-1EX20-0XE0), we need to use STEP7 V5.4 SP4 or higher. I tried it on V5.4 SP5 butgetting the same problem. 2. I am having PCS7 V 7.0(on my workstation) in which STEP7 is of V5.4SP3.If i have to work on STEP7V5.4 SP4 then wat should i do a)upgrade STEP7 V5.4 SP3 to STEP7 V5.4 SP4(is it ok with PCS7) b)uninstall PCS7 and install STEP7 V5.4 SP4. Please help me out. Thanks in advance. AttachmentTest.zip (208 Downloads) |
1/12/2010 7:55 AM | |
Joined: 5/12/2009 Last visit: 6/14/2022 Posts: 13 Rating: (0) |
Thanks Darius. |
Follow us on