Industry Online Support
Technical Forum
7/15/2009 8:32 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (306) |
Hello, When you want to talk native TCP over the PN port of a CPU, you do not configure the connection in NETPRO. The connection description data is in a databloc, and you the so called open IE communication blocks. Here an example: http://support.automation.siemens.com/WW/view/en/29737950 Here another link explaining differnces between TCP over the PN port and over a CP http://support.automation.siemens.com/WW/view/en/24294554 To create the DB with the connection description, there is a wizard available. You can download it from here: http://support.automation.siemens.com/WW/view/en/25209116 |
Best regards |
|