Industry Online Support
Technical Forum
5/12/2008 1:01 PM | |
Posts: 15 Rating: (0) |
Hi! About Rewiring of STEP 7 "SIMATIC Managger" is operated in order to change the input-and-output address of a program. When inputting an address into the screen displayed by "Option--->Rewiring" Please see the appended PDF file. If "I32.0" is inputted with the English notation, it will be set to "Syntax error" and will be refused. "Rewiring" will be carried out if "E32.0" is inputted with the German notation. At "STL Editor", it is working with the English notation. The display of "SIMATIC Managger" also serves as the English notation. Why does it demand the German notation only at the time of "Rewiring"? The version of "SIMATIC Managger" is "V5.2 +SP1 +HF3" Have I made the mistake? Attachmentmelsec.pdf (251 Downloads) |
5/13/2008 3:34 AM | |
Posts: 15 Rating: (0) |
Thank you for a reply. The occurrence which gets confused occurred. The English notation will also be received, once it turns off the power supply of PC and it rises anew. And it was refused with the German notation. The appended PDF file is seen. This PDF file becomes the contents after re-starting PC. Mr. "Pegaia"'s indication matter, There is no setup used as the hindrance of the English notation. "simbolic adress" has not given. A setup when appealing against fault is unknown. It is thought that these setup was wrong. When the same phenomenon occurs, check the setting item which I had taught. Thank you Attachmentmelsec.pdf (216 Downloads) |
Follow us on