9/17/2019 4:00 PM | |
Joined: 4/28/2015 Last visit: 9/20/2022 Posts: 1278 Rating: (295) |
HI; for STEP7 V5.x there is the function block FB283 available: https://support.industry.siemens.com/cs/ww/en/view/25166781 This block can be used with different telegrams. For the different telegrams there are different UDTs available. So there is also one UDT for Tel111. I think that's what you are looking for - have fun with it |
Best regards, |
|
This contribution was helpful to2 thankful Users |
9/24/2019 1:46 PM | |
Posts: 6 Rating: (0) |
Excuse me。。。。 My CPU is 317F-2DP, so I must use CP34-1 moudle connection to V90 servo controller. about this, I can not use FB283 in Step7... Now, in my program CALL FC11 and FC12, transfer data between the PLC and V90. Online PlC and V90, monitor telegram 111, The servo feedback state WORD can be read in PLC DB, But in servo controller , I can not view PLC command WORD. From first word to last word, there are all "0".... |
Follow us on