11/27/2007 2:08 PM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating: (121) |
Hi, in the attachment you will find my constellation. This should be work During the installation from WinCC flexible there are no point like "Integrate in STEP 7". In STEP 7 you create a PC Station. In the configuration you choose the flexible RT and after then the flexible Project are integrated in STEP 7. Notes: WinCC flexible must be installed after the STEP 7 installation. regards, AttachmentPic_01.zip (123 Downloads) |
This contribution was helpful to1 thankful Users |
12/7/2007 3:37 PM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating: (121) |
Hi, |
Follow us on