11/21/2019 1:11 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Yes, user can configure absolute encoder, for more details refer attached sheet.
AttachmentCU250S Vector mode absolute encoder configuration.pdf (132 Downloads) |
11/25/2019 6:31 PM | |
Joined: 8/31/2005 Last visit: 8/20/2024 Posts: 2198 Rating: (328) |
No, the SINAMICS G120 CU250S-2 PN has a built in interface for encoders. (see https://support.industry.siemens.com/cs/ww/en/view/109751322/85824611083) The SMC 10/20/30 modules are for CU320-2 based SINAMICS like G130, G150, S120, S150 |
Last edited by: miami at: 11/25/2019 18:31:28 |
|
11/26/2019 5:24 AM | |
Joined: 6/8/2013 Last visit: 7/18/2024 Posts: 158 Rating: (9) |
Hi Miami, ABSOLUTE VALUE ENCODER 6FX2001-5FS24 MULTITURN 25 BIT WITH SSI, OPERAT. VOLT. 10-30 V SYNCHROFLANGE SHAFT 6MM RADIAL FLANGE SOCKE. The above encoder is suitable for CU250s. Thanks |
11/26/2019 10:52 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Please expalin what you want to track for results? |
Follow us on