8/22/2020 1:16 AM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
Very good question as it happens an interesting discussion is considering that very same question. |
8/23/2020 11:47 AM | |
Joined: 3/30/2020 Last visit: 4/18/2024 Posts: 4412 Rating: (924) |
Hello Kal.A, There is no such thing
Note "timer1" is only as check circuit. It was used to confirm correct functionality. As luck would have it, I need something like this for a simulation circuit. This code will be used (slight changes) to simulated encoder pulses. BR Attachmentretentive-absolute-time.txt (66 Downloads) |
Last edited by: qwazee at: 08/27/2020 06:42:27Caution: The code is flawed. Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to1 thankful Users |
Follow us on