5/24/2006 7:14 PM | |
Posts: 3149 Rating: (171)
|
Hi, perhaps will give this FAQ some more info: http://support.automation.siemens.com/WW/view/en/70775 you should check as well the WinCC release notes. nemo |
5/31/2006 9:38 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (151)
|
If you have a Client Without Project the security is configured on the server project and works on the client as well. If you have a Client With Project ( multi-project ) then you need to recreate the settings in the User Administrator on the client. So recreate all the users and access levels. If you wantcentralised security across all clients and servers you can use the Simatic Logon Option for WinCC. You can find more information about this option at http://www.siemens.com/wincc/options and select Simatic Logon from the navigation bar. |