1/9/2009 12:52 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello Abhijeet.DK, Start with this FAQ: What identification data can I read out of SIMATIC S7 CPUs? There has also links to helpfull manuals... regards |
1/15/2009 10:54 AM | |
Posts: 6 Rating: (1) |
PLEASE LET ME KNOW HOW TO CONFIGURE SFC51 IN S7 |
1/19/2009 2:05 PM | |
Joined: 1/4/2008 Last visit: 9/2/2024 Posts: 703 Rating: (96) |
Hello, here is the STL source with SFC51 configuration for individual LED status in the attachment... But take care about data validity, the data are valid when #Busy is zero and I suppose to trigger the SFCcalling, because continuous calling can cause bigger load for CPU (it means longer execution time of user program cycle). AttachmentFC_LED_DIAG.zip (355 Downloads) |
1/23/2009 11:10 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello See this example: How can you read out the serial number of the MMC? Use the same way and information from this link http://support.automation.siemens.com/WW/view/en/22742674 . Hope this will help you! regards |
Follow us on