11/29/2011 3:43 PM | |
Joined: 7/7/2010 Last visit: 9/19/2024 Posts: 15207 Rating: (2417) |
Once solution is to configure your router to forward a different port from the internet to port 80 on the PLC's IP address. Let's say your router is at www.myPLC.com and your PLC address is 192.168.1.100. You configure the router to forward port 8080 to ip address 192.168.1.100. You connect to your PLC at http://www.myPLC.com:8080/ Hope that makes sense. If you have port 80 of the router open on the internet to edit the router itself, that could be a potentially bad thing if some kid running a hacking script on your router tries to break in. Most routers are programmable from IP addressesinside the LAN only and not from the internet. |
science guy |
|
12/20/2012 5:05 PM | |
Joined: 1/23/2009 Last visit: 7/20/2024 Posts: 29 Rating: (10) |
Dear SOTOSQ, I made s71200 web server connection over internet... Work great Please visit another subject in s71200 forum: How can I access remotely to the S7 PLC 1200? there is a strep by step explanation on page 3..... Greetings..... |
Be creative while inventing ideas and be disciplined while implementing them... :) |
|
11/20/2015 2:10 PM | |
Joined: 8/3/2009 Last visit: 9/2/2024 Posts: 4 Rating: (0) |
Thank you very much! |