Industry Online Support
Technical Forum
8/19/2008 11:06 PM | |
Posts: 49 Rating: (5) |
I do a lot of this, I don't seem to get the foreign travel any more :( Firstly, as has been said, make sure that you can access the PLC from the local network. The CP doesn't seem to autosense, so you'll need to plug into a router or a hub, or use a 'crossover' ethernet lead. then connect MicroWin by selecting the interface and the IP address. Once you've connected locally, ensure that port 80 and port 102 are forwarded to the CP243-1 IT in the router and then try remote access. We have a CP 243-IT online as a demo at http://s7-200.germainesystems.eu you are welcome to use it, get in contact if you want programming access. Best Regards Marc Sinclair |
Follow us on