7/21/2015 12:47 PM | |
Posts: 47 Rating: (0) |
Hi , I am also trying to acheive the position status for which i have set P 734.1 = 120 and p 734.2 = 120 , However i am getting high counts in my input words and it goes above high value of double word very easily even though the drive has not moved much distance Am i missing some thing Can u pls post a snap shot of things to do and what parameters need to set . When i give set point for speed it operates correctly but for position status i dont get it correctly
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/21/2015 2:16:36 PMNew subject after splitting |
|
7/21/2015 2:18 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4775 Rating: (123) |
|
Follow us on