10/11/2011 11:36 AM | |
Posts: 118 Rating: (4) |
Hi I got one situation to trigger the PLC to stop mode. I am trying to achieve SCADA redundancy with the following system ( IFix SCADA <-> Kepware -> S7400H CPU). Now, we have another plan, when CP443 in Rack0 got failed, we have to switch the Rack1 CPU to Master. So that Kepware can connect Rack1 CPU with CP443 in the same Rack. Splitted from Force S7 400H switch between Standby and Master CPU . |
Last edited by: O_Moderator at: 10/11/2011 11:49 AMnew subject after splitting |
|
10/11/2011 11:49 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Thread closed, because question is already discussed in the following thread IFix SCADA <-> Kepware -> S7400H CPU. Best regards O_Moderator |
Follow us on