Industry Online Support
Technical Forum
4/21/2008 10:01 AM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating: (121) |
Hi, i mean you can use the function from the "Alarm View" under "properties > Security > Runtime Security". Orcreate a own "ACK Button" Use a Tag under properties > animations > visibility If a fault message displayed, then you displaying the "ACK Button" The Fault messagemust be acknowled from the PLC: -> http://support.automation.siemens.com/WW/view/en/19439876 regards, |
4/21/2008 12:43 PM | |
Posts: 23 Rating: (0) |
I solved it by setting authorization on the Alarm view popup window and added <tag username> to all of my alarms. |
4/22/2008 9:14 AM | |
Posts: 218 Rating: (28) |
If this was WinCC it would've been so easy to do. Wonder if Siemens will implement this in next releases....... |
4/22/2008 2:19 PM | |
Joined: 5/8/2006 Last visit: 4/19/2024 Posts: 1085 Rating: (77) |
Hi, I think that is easy in WinCC flexible, too. Bye |
Follow us on