3/15/2007 7:28 AM | |
Joined: 2/5/2007 Last visit: 9/9/2023 Posts: 101 Rating: (10) |
Thanks. I've read about it and this is perfect. -- Daniel |
3/15/2007 9:18 AM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8615 Rating: (1147) |
Hi Daniel, I'm glad I could be of some help. Best regards, Wizard |
3/23/2007 6:48 PM | |
Joined: 3/3/2006 Last visit: 11/10/2023 Posts: 28 Rating: (0) |
Hello! |
5/15/2007 10:22 PM | |
Posts: 6 Rating: (0) |
I want to use the "Acknowledge from PLC" setting in WinCC Flexible 2005 (SP1 HF6) to transfer alarm acknowledgements from one console to other consoles. Whenever I try to enter a tag in the "Acknowledgement PLC" field of the Discrete Alarm, the field turns orange and I get the error mesage "This value is invalid" (see attached pdf). There is nothing in the help to explain this and the previously posted solution does not have this problem. Please help. What am I missing? AttachmentDiscreteAlarm.pdf (145 Downloads) |
5/16/2007 7:08 PM | |
Posts: 6 Rating: (0) |
G.John - thanks for the help, but.... I tried the exact same tag & bit but get the same "invalid tag" message (see attached pdf). Also, when I browse for a PLC acknowledgement tag I only get one word shown in the list of tags available but browsing for the HMI acknowledgement tag I get the full list of all tags. Does the acknowlegement tag have to meet some special criteria? Thanks. AttachmentAlarmAckPLCTag.pdf (148 Downloads) |
Follow us on