10/8/2010 8:40 PM | |
Joined: 7/28/2010 Last visit: 3/18/2024 Posts: 184 Rating: (11) |
Hi, If your values are collected in the script then you have tocall the script to update the values as script is even triggered and doesn't get called automatically. If the values are collected in the screen, then that happens automatically as long as it is set to continuous. I think it is better to call your scriptby a tag from plc based on the intervals you want, lets say every 0.5 sec or 1 sec and collect all data in the script and pass it to your database. Regards, Behnam www.sigmaprocess.ca/blog |
Follow us on