10/28/2021 7:34 AM | |
Joined: 9/9/2014 Last visit: 10/5/2023 Posts: 73 Rating: (0) |
Hello, i have similar situation for Action (Technological) that not working as it should be. i use PCS7 V9.1 with SFC V9.0+SP5+Upd2 Attached the action i mentioned, it should execute the action of StartAut of MotL block and reset the command in termination. However, during testing the action intended not working. Anyone have any suggestion to resolve the issue? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: mr Gun at: 10/28/2021 07:38:24Last edited by: The Helping Hand at: 10/28/2021 08:35:11New subject after splitting |
|
10/28/2021 2:28 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi, Your print screens are not clear. I don't see where you are using StartAut etc. What you should do: 1. Create a CMT with a technological block like VlvL, MotL etc. 2. In the CMT, create commands like SetStart. When configuring the SetStart, select the desired block contacts from the list. You can configure StartAut.Value :=TRUE in Initialization/Processing and StartAut.Value :=FALSE 3. After configuring the commands (and statuses like IsAuto or IsRunning), create a role assignment in the EPHT/EMT and insert the CMT as template with option: Basic requirement enabled. 4. Assign the role assignment to the template and now you can use it in the SFC of the EPHT/EMT 5. Configure the technological action in the SFC and assign the command like SetStart. You won't need to use the "old school" Initialization/Processing/Termination" tabs but only the technological actions/conditions. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on