1/14/2008 2:24 PM | |
Joined: 2/22/2006 Last visit: 9/21/2024 Posts: 74 Rating: (3) |
Hi, here are the logs from my test-pc. As it happens on this pc too, I think the problem is within the project and not on the pc. You don't have any incompatible software in those computers, right? >> I don't think so. You said the projects have the same "base engineering"... does this mean someone created a project, then you deleted the data from the old project to start this one? Or do you have a basic application, with basic features, and use it for all projects? >>once we made a project, and for the next one we took the old and modified it, ... Were all projects created / edited under the same WinCC version? >>Starting was with V60+SP2, now the two projects with this failure ar V60+SP3 and V60+SP4. You said you think you think it's a 24 days interval... Do all computers fail at the same time, or do they fail with the same time interval? >>It's not always this intervall. On my test-pc the break was after 2 days, and now it is running since 10.1. Thanks AttachmentPIO5000.zip (126 Downloads) |
Last edited by: Franschitz at: 14.01.2008 14:27I've forgot one think: what is the CCRtsLoader.exe? |
|
3/7/2008 7:09 PM | |
Posts: 1275 Rating: (123)
|
Hi, Have you tried contacting technical support for this? They may help! Best regards, Danielle |
3/11/2008 12:35 PM | |
Posts: 1275 Rating: (123)
|
OK... Please let us know how that works! Good luck.. Danielle |
Follow us on