2/5/2015 10:31 AM | |
Posts: 3609 Rating: (29) |
Import of a technical question from the user jrm1966:
|
8/27/2021 3:15 PM | |
Joined: 4/5/2020 Last visit: 9/27/2023 Posts: 29 Rating: (0) |
this is very easy just follow to the following steps on the face plate configuration select a button which want to navigate you to other screen its up to you if want to click then drag and drop the click property of the Button then drop it to the face plate EVENT INTERFACE then when you use a face plate any where just go to the event property then chose a function as you want , for my case i used ACTIVATE SCREEN see the attached Rate if its helpful AttachmentFP_SCREEN_NAVIGATION.pdf (329 Downloads) |
Follow us on