Industry Online Support
Technical Forum
8/18/2010 1:29 PM | |
Posts: 39 Rating: (0) |
Hello, I am facing a problem with the activation and deactivation of a drive with SIMOTION and Sinamics Integrated version V4.1 SP4 SINAMICS IntegratedPN2.2 V2.5 If I activate or deactivate both the drives on that particular DMM then the remainng drives on SINAMICS Integrated come online. If I deactivate only one drive on the DMM, all the drives on SINAMICS Integrated show me the error of Drive-Cliq communication.Both the LEDs become orange on the DMM. Now, Is this a problem of the firmware being used or the procedure? I am deactivating the drive using parameters 105,125 and 145 on the drive and also tried to deactivate the TO in SIMOTION. ___________________________________________________________________________ Secondly, I want to change the SINAMICS Integreted version to PN2.2 V2.6 Now if I visit the particular link for SIMOTION kernel then there is no version availbale for V2.6 SINAMICS Integrated http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csSearch&objaction=cssearch&lang=en&siteid=cseus&query=&query2=Sinamics%20Integrated%20V2.6&content=adsearch%2Fadsearch%2Easpx But in this following document it mentions of SINAMICS V2.6.2 but then why is the firmware not available on the link above? SUPPORTING DOCUMENT: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=37841397&objAction=csOpen&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW ________________________________________________________________________________ Please help me out. Regards |
8/18/2010 2:33 PM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011)
|
Hello, second first: in the V4.1.4.1 Kernel with SINAMICS V2.6 there a big Bug with saftey so the kernel is not longer delievered. You can use SIMOTION V4.1.5.3 with SINAMICS V2.6 To the first question: which values do you have used for 105, 125, 145? Is the DMM which you have deactivated the last in the DQ Line? Which part of the DMM do have disabled?(X1 or X2)? Regards Christoph |
8/19/2010 11:55 AM | |
Posts: 39 Rating: (0) |
Hello Thankyou for your advice and the problem has been resolved. We did not change the firmware but instead we just changed the parameter no in 105,125 and 145 as 1 (Deactivate drive object) instead of 2.(deact and not present) _____________________________________________________________________________ Problem: One Cu320 is present along with 2 DMMs. the drives on X2 connection on both DMMs have be deactivated. Now whenever we try to open the topology an error pops up which is shown as a screenshot in the attachment. There is a topology warning "Additional Component present". Is this because the firmware upgradation has not taken place on that drive or we have to set some parameters. Please help us on this too. _____________________________________________________________________________ Now we have certain queries which you can guide us: 1. During firmware upgrade what is the procedure to be followed if there is one particular motor absent from the DMM? Are there any steps to be followed? Since we are not connecting a motor on the second connection how do we get the firmware upgrade for that particular drive on the DMM? 2. Earlier machine had version V04.01.01.06 where we used no 2 (deatctivate and not present) for deactivation and activation on the same DMM Sinamics Integrated 02.50.32.16 there this problem did not occur. The only chage we have made is of the firmware in this machine which is V4.1 SP4 PN2.2 V2.5. Can this be due to the firmware? 3. What is the difference between Deactivate drive object no.1 and deactivate and not present no.2? 4. Do we have to follow the same procedure for SINAMICS other than SINAMICS Integrated? 5. Topology error occurs when this particular problem exists and I have attached a screenshot for your reference? How can we overcome this and why does this happen? If this screen is there we cannot open the topology screen and nothing can be viewed! 6. Placement of the DO in the line does it make a difference ? ___________________________________________________________________________ Regards. AttachmentSinamics_Int_topology_error1.zip (208 Downloads) |
Follow us on