6/20/2013 3:53 PM | |
Joined: 10/7/2005 Last visit: 9/20/2024 Posts: 3021 Rating: (1054)
|
Hello KonradR I agree that at the moment in time when you noted down the status of the preceding logic, M129.0 will NOT be actively set to 1 (the RLO that drives the SET operation for M129.0 will be zero since I0.5 is zero) . Having said that, M129.0 is set tovia a - well - "S" (SET) operation and could have been latched on long before you noted down the status of the preceding logic. As such it will of course remain set even if the logic before it does not actively set it anymore. Reset M129.0 manually and I'm sure it will remain0, so thequestions really is: What logic will reset M129.0? I hope this helps |
Cheers |
|
This contribution was helpful to2 thankful Users |
Follow us on