7/13/2021 9:49 AM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33003 Rating: (4078)
|
And why do you make your topic in a LOGO! conference? |
7/15/2021 4:27 PM | |
Joined: 4/28/2015 Last visit: 1/19/2024 Posts: 13 Rating: (1) |
Hello xhamist, I guess you are using one of the Baumer IO-Link Master PROFINET https://www.baumer.com/pl/en/product-overview/cable-connectivity/io-link-master/c/38920 For example in operating manual of 8-Port, IP67 device, you can find description (chapter 10) to read/write data with cyclic communication. For reading inputs via data records there is also a description of data records index numbers to use Excerpt: Index Description 100..131 1 - 32 byte of PDI data from an IO-Link Port module in Slot 1 200..231 1 - 32 byte of PDI data from an IO-Link Port module in Slot 2 300..331 1 - 32 byte of PDI data from an IO-Link Port module in Slot 3 How to use _readRecord() function you can find in SIMOTION online help or documentation like "system functions/variables devices)https://support.industry.siemens.com/cs/ww/en/view/109767607 |
Follow us on