3/29/2019 8:57 AM | |
Joined: 4/28/2015 Last visit: 1/4/2024 Posts: 36 Rating: (1) |
Hi! I have the same problem, three DMM and one SMM, thats a total of 7 and to much. The system was with two DMM and one SMM in the first version. No problem. Now, i had to add to axes but the TIA v14 wont let me download the new configuration beacuse it is now 7 objects. The DMM module wich has only one motor is deactivated. How can I proceed? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/29/2019 11:34:33 AMNew subject after splitting |
|
3/29/2019 11:53 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Disable one motor is published within the conference SINAMICS. Best regards Jen_Moderator |
Follow us on