8/3/2020 10:46 AM | |
Joined: 5/12/2006 Last visit: 4/18/2024 Posts: 22207 Rating: (2979) |
anf about which tool you talk? |
8/3/2020 3:59 PM | |
Posts: 7 Rating: (0) |
yes, Simatic Automation Tool v4 |
8/3/2020 4:04 PM | |
Posts: 7 Rating: (0) |
So it's not possible to add (knowing its ip address) a CPU that is not in the same subnetwork ? |
8/3/2020 4:58 PM | |
Joined: 3/28/2015 Last visit: 4/14/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following topic might help: |
Eng.Mohamed Ibrahim |
|
8/4/2020 8:51 AM | |
Posts: 7 Rating: (0) |
I don't have a problem with this step, my problem is the following, I can't add equipment from different subnets. |
8/4/2020 8:53 AM | |
Joined: 5/12/2006 Last visit: 4/18/2024 Posts: 22207 Rating: (2979)
|
the answer is given in the post from Mops04. can only work in the same subent because no-routable protocol is used. |