12/12/2017 9:47 AM | |
Joined: 5/21/2017 Last visit: 5/20/2019 Posts: 11 Rating: (0) |
Dear all, I have a SIMOTION Scout project v4.1 (SIMOTION D445) which I converted and saved in the new version with SIMOTION SCOUT v4.4. The HMI part was 'Copied from Step7' in WinCC flexible 2008 SP3 Advanced and then migrated to TIA project. (Version V13 SP2). Then, I added a device proxy in TIA and tried to intialize using the SIMOTION project (.mcp file) but it gives the error "No CPU or defined device proxy data were found." I tried initializing with the TIA project (.ap13 file) but it gives the same error. Is there something else that has to be done? Any advise/suggestion would be really helpful. Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/12/2017 1:02:53 PMNew subject after splitting |
|
2/18/2018 7:42 AM | |
Joined: 5/21/2017 Last visit: 5/20/2019 Posts: 11 Rating: (0) |
Hello, Is there any other way? Awaiting the expert's opinion to proceed. Thank you. |
6/6/2018 2:59 AM | |
Joined: 1/19/2017 Last visit: 5/4/2023 Posts: 1 Rating: (0) |
Hello, I had the same problem. Is there any solution? Thank you very much. |
Follow us on